No application file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No application file

3,267 Views
juliancox
Contributor V

I have developed an application  using CW11.1 with a S08SH8 and everything was fine - it compiled and I could debug it using my Multilink FX. I have just made a minor software change. It complies without errors but I cannot debug it. I get the message: -

Application file not specified in the launch configuration

In the Debug Configuration dialogue the Application box is ticked and the file is FLASH/DEO_01_Issue_7F.abs.

However, no  ---abs or ...abs.s19 file has been generated. Other applications in the workspace are OK.

0 Kudos
Reply
7 Replies

3,118 Views
BlackNight
NXP Employee
NXP Employee

Make sure that the file FLASH/DEO_01_Issue_7F.abs is present (check your build). Maybe it failed because of an error.

If your build produces a different output file name, then update your launch configuration to match that name.

I hope this helps,

Erich

0 Kudos
Reply

3,118 Views
juliancox
Contributor V

Yes, the .abs and the .abs.args files are present and all files have the same name. Just to confirm, the build process completed without errors and displayed the following line in the console window: -

'Finished building target: DEO_01_Issue_7F.abs'

0 Kudos
Reply

3,118 Views
BlackNight
NXP Employee
NXP Employee

Are the files visible in the Project Explorer? If not, press F5 (Refresh) as Eclipse might not have refreshed the view with the changed disk content.

I hope this helps,

Erich

0 Kudos
Reply

3,118 Views
juliancox
Contributor V

The s19 file is not present because it is not being generated. Referring back to my original problem, this is the message i get:

pastedImage_1.jpg

yet the application file is specified and it does have the correct name.

What I do not know is will the lack of a s19 file cause this error?

regards,

Julian

0 Kudos
Reply

2,767 Views
Rameshtrolex
Contributor I

Am also facing the same isues

0 Kudos
Reply

3,118 Views
BlackNight
NXP Employee
NXP Employee

Hi Julian,

would it be possible to share your project which reproduces this?

Remove your (confidential, if any) source files. All what is needed is something to reproduce what you see.

Erich

0 Kudos
Reply

3,118 Views
juliancox
Contributor V

Hi Erich,

"Cheer up, they said - things could be worse. So I cheered up and things got worse."

Before sending you my project I thought I would create a new project and see what happened. This time I got about 10 errors._

"Cannot find xxx.h"  where xxx was a ProcessorExpert component. At this stage I thought that CW was gradually destroying itself.  Then I tried to run an example project and got the original error.

I then uninstalled CW 10.7, rebooted Windows and reinstalled CW. After a bit of tidying up I now have everything working. I have not yet installed the 10.7 service pack and I may reinstall CW 11 (just to be safe). 

Finally, thanks for your help.

0 Kudos
Reply