Hi all ,
I am new to Code Warrior ide and Kinetis microcontrollers. Have so many doubts regarding to it.
1. What is Clean and when we clean what happens in the background ?
2. What is the difference between build all and build project ?
3. What is mean by .afx file ? how to create it and when to create it ?
4. What is mean by .elf file or .abs file and how to create it ?
5. Which file to be loaded into the target for debugging ?
6. What are S19 files (S-record files) ? When they are created during the compilation process ?
7. Need to study about the MQX rtos from basic, Which guide to follow ?
Please help with the above questions and also mention the reference file from where you have got it ?
Most of all, If I need to know the meaning of all the words that are used in the Code Warrior IDE , Which Guide or Manual I need to refer to get the answer for all the words.
Thanks in Advance
Siva Kumar A