Mysterious Compile Error with NV_data.c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Mysterious Compile Error with NV_data.c

跳至解决方案
5,048 次查看
ArtLab
Contributor I

Hello,

 

I'm having difficulty compiling code for the MC13213 where I wasn't before.  I know errors don't magically appear, but I'm at a lost with this one.

 

The compile error points to the NV_Data.c file.  Neither I, nor to my knowledge other programmers on this project, have changed this file.  I've copied the error messages below and the block of code it points to.  I'm not sure if this error points to some other configuration problem in my codewarrior 5.9.0 project. I hope this is something simple that someone on this board can help me solve. 

 

thanks,

 

ArtLab

 

 

/***********Code block with error*******************/

 

/*****************************************************************************
******************************************************************************
* Public functions
******************************************************************************
*****************************************************************************/

/*****************************************************************************
* locates the NV RAM to use.There are 2 NVM sectors.It sets apointer to
* valid sector.   
*
* Interface assumptions:
*
* Return value:
* None
*
* Revison history:
*
* date   Author   Comments
* ------ ------   --------
* 290301 FSL,ANP  Created
*****************************************************************************/

void NVM_FindNVRAM( void )
{
    NvramSectorStruct_t * pSectorStruct;
    NvramStruct_t *pMacStruct;

  uint16_t iCounter = 0;
  
  uint8_t mac[4] = "MAC";
    uint8_t zs1[4] = "ZS1";
    uint8_t zs2[4] = "ZS2";
  /* Array of pointers to NVM Sectors  */
  void * apSectors[4] = { pStoredNvram0_c, pStoredNvram1_c, pStoredNvram2_c, pStoredNvram3_c};
 
     
    gpMacNvram = NULL;        /*  MAC NVRAM Not found */
    gapBeeStackNvram[0] = NULL;
    gapBeeStackNvram[1] = NULL;
    gpScratchPadNvram = NULL; /*  SP NVRAM Not found  */

   /* loop to find the corresponding NVM sector */
    for( iCounter = 0; iCounter < 4; iCounter++ ){
   
      pSectorStruct = ( NvramSectorStruct_t * )( apSectors[ iCounter ] );
      pMacStruct =  ( NvramStruct_t * )( apSectors[ iCounter ] );
   
      if( FLib_MemCmp(( void* )pSectorStruct->aString,
        ( void* )zs1, 3 ))  {
        gapBeeStackNvram[0] = ( NvramSectorStruct_t * )( apSectors[ iCounter ]);
      }
      else if( FLib_MemCmp(( void* )pSectorStruct->aString,
        ( void* )zs2, 3 )) {
        gapBeeStackNvram[1] = ( NvramSectorStruct_t * )( apSectors[ iCounter ]);
      }     
      else if( FLib_MemCmp(( void* )pMacStruct->MAC_Version,
        ( void* )mac, 3 )) {
        gpMacNvram = ( NvramStruct_t * )( apSectors[ iCounter ]);
      }
      else  {
         gpScratchPadNvram = ( void * )( apSectors[ iCounter ]);
      }
    }   
 return;
}
/***********************************************/

 

/**************ERROR Messages******************/

Error   : C2207: Initializer must be constant

NV_Data.c line 327  

Error   : C1815: NvramSectorStruct_t not declared (or typename)

NV_Data.c line 338  

Error   : C2450: Expected:  . * + - & ! ~ ++ -- -> [ (  IDENT CONSTANT STRING sizeof __alignof__ __va_sizeof__ __va_arg_type__   

NV_Data.c line 338  

Error   : C1827: Arithmetic types expected

NV_Data.c line 338  

Error   : C1844: Call-operator applied to non-function

NV_Data.c line 338  

Error   : C1822: Type mismatch (expected 'NvramSectorStruct_tag *', given 'error ')

NV_Data.c line 338  

Error   : C1806: Illegal cast-operation

NV_Data.c line 338  

Error   : C1815: NvramStruct_t not declared (or typename)

NV_Data.c line 339  

Error   : C2450: Expected:  . * + - & ! ~ ++ -- -> [ (  IDENT CONSTANT STRING sizeof __alignof__ __va_sizeof__ __va_arg_type__   

NV_Data.c line 339  

Error   : C1827: Arithmetic types expected

NV_Data.c line 339  

Error   : C1844: Call-operator applied to non-function

NV_Data.c line 339  

Error   : C1822: Type mismatch (expected 'NvramStruct_tag *', given 'error ')

NV_Data.c line 339  

Error   : C1806: Illegal cast-operation

NV_Data.c line 339  

Error   : C2801: ')' missing

NV_Data.c line 341  

Error   : C2801: ';' missing

NV_Data.c line 342  

Error   : C1814: Arithmetic or pointer-expression expected

NV_Data.c line 343  

Error   : C1815: NvramSectorStruct_t not declared (or typename)

NV_Data.c line 343  

Error   : C2450: Expected:  . * + - & ! ~ ++ -- -> [ (  IDENT CONSTANT STRING sizeof __alignof__ __va_sizeof__ __va_arg_type__   

NV_Data.c line 343  

Error   : C1827: Arithmetic types expected

NV_Data.c line 343  

Error   : C1844: Call-operator applied to non-function

NV_Data.c line 343  

Error   : C1822: Type mismatch (expected 'NvramSectorStruct_tag volatile *', given 'error ')

NV_Data.c line 343  

Error   : C1806: Illegal cast-operation

NV_Data.c line 343  

Error   : C2801: '}' missing

NV_Data.c line 345  

Error   : C2801: ')' missing

NV_Data.c line 345  

Error   : C2801: ';' missing

NV_Data.c line 346  

Error   : C1814: Arithmetic or pointer-expression expected

NV_Data.c line 347  

Error   : C1815: NvramSectorStruct_t not declared (or typename)

NV_Data.c line 347  

Error   : C2450: Expected:  . * + - & ! ~ ++ -- -> [ (  IDENT CONSTANT STRING sizeof __alignof__ __va_sizeof__ __va_arg_type__   

NV_Data.c line 347  

Error   : C1827: Arithmetic types expected

NV_Data.c line 347  

Error   : C1844: Call-operator applied to non-function

NV_Data.c line 347  

Error   : C1822: Type mismatch (expected 'NvramSectorStruct_tag volatile *', given 'error ')

NV_Data.c line 347  

Error   : C1806: Illegal cast-operation

NV_Data.c line 347  

Error   : C2801: '}' missing

NV_Data.c line 349  

Error   : Compile failed

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,587 次查看
CompilerGuru
NXP Employee
NXP Employee

For any kind of mysterious compilation error in C, always check the preprocessor output.

If the preprocessor output on its own does not help you, save it as *.c and compile it, so the compiler

refers into it for its error message.

Maybe some name conflict in a included file.

 

Daniel

BTW: As note to the code, you could make the arrays static const so the compiler does not have to create

them on the stack, e.g.

static const uint8_t mac[4] = ...

static void * const apSectors[4] ={..

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,588 次查看
CompilerGuru
NXP Employee
NXP Employee

For any kind of mysterious compilation error in C, always check the preprocessor output.

If the preprocessor output on its own does not help you, save it as *.c and compile it, so the compiler

refers into it for its error message.

Maybe some name conflict in a included file.

 

Daniel

BTW: As note to the code, you could make the arrays static const so the compiler does not have to create

them on the stack, e.g.

static const uint8_t mac[4] = ...

static void * const apSectors[4] ={..

 

0 项奖励
回复
3,472 次查看
w_lingjun
Contributor III

Hi,

When I transplant a project from CW6.3 to CW11.1, I encountered similar problem. The build problems are as below. I try to save related files as *.c, but it is no effect. Is there any method to resolve the problem?


C1815 TIME_1MIN not declared (or typename) fault.c /ABC210_CT_SX005/Sources line 297 C/C++ Problem
C2801 ';' missing fault.c /ABC210_CT_SX005/Sources line 302 C/C++ Problem
C1801 Implicit parameter-declaration for 'CheckTickTime' fault.c /ABC210_CT_SX005/Sources line 153 C/C++ Problem
C1801 Implicit parameter-declaration for 'TickTime' fault.c /ABC210_CT_SX005/Sources line 217 C/C++ Problem
C1814 Arithmetic or pointer-expression expected fault.c /ABC210_CT_SX005/Sources line 314 C/C++ Problem
C2801 '}' missing fault.c /ABC210_CT_SX005/Sources line 322 C/C++ Problem
C2801 ')' missing fault.c /ABC210_CT_SX005/Sources line 314 C/C++ Problem
C2450 Expected: { IDENT auto break case const continue default do extern for goto if register return static switch typedef volatile while __asm __interrupt fault.c /ABC210_CT_SX005/Sources line 314 C/C++ Problem
C1801 Implicit parameter-declaration for 'CheckTickTime1Ms' time.c /ABC210_CT_SX005/drive line 62 C/C++ Problem
C2801 ';' missing time.c /ABC210_CT_SX005/drive line 89 C/C++ Problem
C1814 Arithmetic or pointer-expression expected time.c /ABC210_CT_SX005/drive line 90 C/C++ Problem
C1815 TICK_TIME_LIMIT not declared (or typename) time.c /ABC210_CT_SX005/drive line 87 C/C++ Problem
mingw32-make: *** [Sources/fault_c.obj] Error 1 ABC210_CT_SX005 C/C++ Problem
C2801 ')' missing time.c /ABC210_CT_SX005/drive line 89 C/C++ Problem
mingw32-make: *** Waiting for unfinished jobs.... ABC210_CT_SX005 C/C++ Problem
mingw32-make: *** [drive/time_c.obj] Error 1 ABC210_CT_SX005 C/C++ Problem
C1814 Arithmetic or pointer-expression expected fault.c /ABC210_CT_SX005/Sources line 326 C/C++ Problem
C2450 Expected: { IDENT auto break case const continue default do extern for goto if register return static switch typedef volatile while __asm __interrupt fault.c /ABC210_CT_SX005/Sources line 326 C/C++ Problem
C2801 ')' missing fault.c /ABC210_CT_SX005/Sources line 326 C/C++ Problem
C2801 ';' missing fault.c /ABC210_CT_SX005/Sources line 324 C/C++ Problem
C2801 '}' missing fault.c /ABC210_CT_SX005/Sources line 335 C/C++ Problem
C2801 ';' missing fault.c /ABC210_CT_SX005/Sources line 332 C/C++ Problem

 

Best regards,

Sarah

0 项奖励
回复