Mix C and assembly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mix C and assembly

5,203 Views
admin
Specialist II
My problem is how to define a variable that can be use in multi C files and assembly files at a application.
 
I define a variable in the first C file, for example:
/* file1.c*/
int i;
 
now I want this variable can be used in another C file and a asm file, for example:
/* main.c*/
#include "file1.c"
main()
{
  i=0;
}
 
/*main.asm*/
XREF i;
...
LDD #0
STD i
 
but it can not be link correctly withing CW for HCS12 v3.1.
 
Please help me!
 
Labels (1)
Tags (1)
0 Kudos
Reply
10 Replies

2,329 Views
Lundin
Senior Contributor IV
The linker error is likely there because you are including a c-file. Never do that, you should only include h-files. This is how it is done properly:

/* file.h */
extern int i;


/* file.c */
#include "file.h"
int i;


/* main.c */
#include "file.h"

int main()
{
i=0;
}


/* file.asm */

XREF i
0 Kudos
Reply

2,329 Views
CrasyCat
Specialist III

Hello

What is the message the linker generates?

CrasyCat

0 Kudos
Reply

2,329 Views
admin
Specialist II

Yeah, I placed the variable "i" in the .h file.

First, I do not use "extern", and the linker note "Link Error : L1818: Symbol - i duplicated in file1.c.o and main.c.o".

Then I added "extern", linker show "Link Error: L1822: Symbol i in file ...file.asm.o is undifined".

0 Kudos
Reply

2,329 Views
Lundin
Senior Contributor IV
You didn't do as shown in my example then. Did you add it to the .c file?


If you declare a variable as

int i;

as shown in my example it -will- be global and every other file in your project can access it. Unless you use the "static" keyword. This is very basic C knowledge.

And XREF works just fine - I'm also using CW3.1 for HCS12.
0 Kudos
Reply

2,329 Views
admin
Specialist II

I notice the different between your sample and mine:

Declare "i" in the h file as "extern", and be included in the two c file, alse be included in the asm file.

I notice that in the first c file you re-declare the variable "i", then everythink ok!

I just wondered whether the two "i" (file.h and file.c) share the same RAM space?

Could you explare it for me?

Thank you!

0 Kudos
Reply

2,329 Views
Lundin
Senior Contributor IV
When you type extern in front of the variable, you aren't declaring the actual variable. You just tell the compiler that we have a variable called 'i' but it is allocated elsewhere. By doing so, every c-file that includes the h-file gets the info that 'i' exists.

Note however that you should place the "extern" in the same memory segment as the variable:

/* file.h */

#pragma DATA_SEG MY_RAM
extern int i;


/* file.c */

#pragma DATA_SEG MY_RAM
int i;
0 Kudos
Reply

2,329 Views
admin
Specialist II

I got it!

Thank you again!

0 Kudos
Reply

2,329 Views
admin
Specialist II
Thanks a lot!
 
I am now declare i in a *.h file:
/* file.h */
int i;
 
and be included and used in file.c, main.c and file.asm:
/* file.c */
#include "file.h"
void file()
{
  i = 0;
}
 
/* main.c */
#include "file.h"
void main()
{
  i = 1;
}
 
/* file.asm */
  XREF i
  LDD #0
  STD i
 
but if I declare "i" as a global variable in the h file, linker show "i" be duplicated by the two c files;
if i declare as extern or static, linker show "i" undefined in asm file.
0 Kudos
Reply

2,329 Views
rocco
Senior Contributor II
Hi, Markie:

Since I don't use CodeWarrior, I can't test this, but it looks like a problem of scope.

In "file1.c", it looks like the variable "i" has file-scope. It does not exist outside of the file "file1.c".

Try declaring it as "global".

Message Edited by rocco on 2006-08-14 02:32 PM

0 Kudos
Reply

2,329 Views
admin
Specialist II
It's seemed that "global" not be supported by CW.
0 Kudos
Reply