MCF51QE128 with SPI(SynchroMaster) Resistive Touch Screen...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51QE128 with SPI(SynchroMaster) Resistive Touch Screen...

531 Views
daltonaota
Contributor I

Good Morning,

 

I wonder if anyone has ever worked with resistive touch screen using SPI(SynchroMaster) ?

 

If yes, you have some source code to help me ?

 

Thank you in advance !

Labels (1)
0 Kudos
Reply
1 Reply

442 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello .

If you download D4D from web page, you will get demo with version 3.0

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=EGUI&fpsp=1&tab=Design_Tools_Tab

inside the package there is a demo for MCF51JM128 which is also Coldfire V1 chip, you can refer it as a start to design your MCF51QE128.

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply