MC68HC08 IS NOT IN CW10.6 LIST

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC68HC08 IS NOT IN CW10.6 LIST

1,073 次查看
peimansh
Contributor II

hi friends

Im install CW10.6 but when I want to create a project, MC68HC08 is not in S08 family list!

whats the problem?

 

regards,

peiman sh.

标签 (1)
0 项奖励
回复
7 回复数

952 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

for which device are you looking for? CodeWarrior supports S08 devices.

Erich

0 项奖励
回复

952 次查看
peimansh
Contributor II

hi,

....MC68HC08AB16A!

which is in s08(cpu08) family.

REGARDS,

PEIMAN SH.

0 项奖励
回复

952 次查看
BlackNight
NXP Employee
NXP Employee

So then can you use that device?

From the tools/compiler perspective there is really no difference between HC08 and HCS08.

Erich

0 项奖励
回复

952 次查看
peimansh
Contributor II

you say right man but there is only MC9HC08A devices in HC08A family,when I want to create a project!

I think MC68HC08A is legacy mcu that is not in cw10.6 any more.

maybe I must insall cw6.3 that is not supported in win7-64bit...

do u have any idea?

regards,

peiman sh.

0 项奖励
回复

952 次查看
takaoyamada
Contributor IV

Greetings,

Erich Styger is correct in that P&E does have a USB-based debugging pod that works with the MON08 chip family, including the MC68HC08AB16A. By using P&E's product, you also are given free MON08 software to flash program and debug your chip. Here is a link to the debugging product:
P&E Microcomputer Systems - USB-ML-MON08 - USB BDM Interface Cable for the 68HC08 MON08 - HC08, Inte...

Here is the software freeware, but you will still need Codewarrior to develop and compile your code:

http://www.pemicro.com/downloads/download_file.cfm?download_id=286

There are work-arounds as Xin Kuang has mentioned with installing CW6.3 and if you plan on using P&E tools we have USB drivers and an unofficial patch I have created for P&E customers to get their P&E hardware working for older Codewarrior classic software on Windows 7 64-bit machines. Here is the FAQ and downloads that you will need:

http://www.pemicro.com/faqs/faq_view.cfm?id=211

I hope my answer was useful for you.

Takao Yamada

P&E Microcomputer Systems

0 项奖励
回复

952 次查看
TICS_Fiona
NXP Employee
NXP Employee

The classic CodeWarrior v6.3 does not support Windows 7. It supports Windows® 98 SE/2000/XP/Vista 32 bits. Below is the link for more details:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MICROCONTROLLERS

There is a completed workaround to install and use it on Windows 7 64-bit machine, please refer to the document below:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf

However there is a P&E driver issue. Customer must download the V10 from P&E web site too.

0 项奖励
回复

952 次查看
BlackNight
NXP Employee
NXP Employee

I have Win7 64bit and no CW6.x any more, as this has been replaced with Eclipse based tools many years ago.

I think the bigger problem will be to debug this HC08 device, as I believe it is using Mon08 interface. You probably even need a PC with a parallel interface as many of the Mon08 debug cables were with Parallel ports. But there was as well a USB based one from P&E. Probably you will need an old XP machine.

Good luck!