解決済! 解決策の投稿を見る。
/************************************************************************************* This file contains some basic linker parameters.** The linker file is made so it matches architecture for the Freescale HCS08 GB60/GT60 ucontroller* to be used in the 802.15.4/Zigbee project. * * This version must be used if the Embedded Bootloader from version 5.00 is on the board. Use old linker file if* you have an older version of the Embedded Bootloader (freeloader) versions before 5.00.** Author(s): Michael V. Christensen** (c) Copyright 2004, Freescale Semiconductor, Inc. All rights reserved.** Freescale Confidential Proprietary* Digianswer Confidential** No part of this document must be reproduced in any form - including copied,* transcribed, printed or by any electronic means - without specific written* permission from Freescale.** Last Inspected: 29-03-01* Last Tested:*************************************************************************************/NAMES// Do not remove this block/section.// Description: The NAMES block contains a list of binary files building the application. This block// is mandatory and can only be specified once in a prm file.// Additional files may be specified by the option -Add. The object files specified with the option// -Add are linked before the files mentioned in the NAMES block. With the option -Add, additional// files can be added to a project without modifying the link parameter file.// If all binary files should be specified by the command line option -add, then an empty NAMES// block (just NAMES END) must be present in the link parameter file. Object files added with this// option are linked before the object files specified in the NAMES block.END// **************************************************************************// Memory map for HCS08 GB60/GT60. All memory areas are define below i.e. registers and stack etc.// are shown.// Options// READ_WRITE is for normal variables// READ_ONLY is for const variables and code// NO_INIT is for uninitialized variables.// Note!// "RES_" means that the system is not allowed to use the specified memory.SECTIONS // Port registers DIRECT_PAGE_REGISTERS = READ_WRITE 0x0000 TO 0x007F; // HW registers - This section contains often used port registers // Fast direct addressable memory DIRECT_ADDRESSING_MEMORY = READ_WRITE 0x0080 TO 0x00FF; // "Fast" RAM memory // 802.15.4/App. stack memory APP_STACK_RAM = READ_WRITE 0x0100 TO 0x025F; // RAM memory // 802.15.4/App. general memory APP_RAM = READ_WRITE 0x0260 TO 0x0102F; // RAM memory CODE_EXECUTION_FROM_RAM0 = READ_WRITE 0x1030 TO 0x01077; // RAM memory RST_APP_VAR = NO_INIT 0x01078 TO 0x01078; // July 28th 05,Lakshmi // Reserve space for NV RAM pointer // The pointer is initialized by code. MAC_NV_RAM_POINTER_RAM = NO_INIT 0x01078 TO 0x01079; // RAM memory ZS_NV_RAM_POINTER_RAM = NO_INIT 0x0107A TO 0x0107D; // RAM memory NVM_SCRATCHPAD_POINTER_RAM = NO_INIT 0x0107E TO 0x0107F; // RAM memory // 802.15.4/App. startup structure flash memory APP_STARTUP_STRUC_FLASH = READ_ONLY 0x01080 TO 0x10AF; // Flash memory // 802.15.4/App. flash memory - section 1 APP_CODE = READ_ONLY 0x010B0 TO 0x17FF; // Flash memory //High page registers HIGH_PAGE_REGISTERS = READ_WRITE 0x1800 TO 0x182B; // HW registers - High page register section APP_CODE_1 = READ_ONLY 0x0182C TO 0x19FF; // BootLoader/802.15.4/App. NV RAM flash memory. // Initialized by 802.15.4. NVM_SCRATCHPAD = READ_ONLY 0x01A00 TO 0x1BFF; // Flash memory BOOTLOADER_MAC_NV_RAM = READ_ONLY 0x01C00 TO 0x1C8C; // Flash memory BOOTLOADER_PHY_NV_RAM = READ_ONLY 0x01C8D TO 0x1CBB; // Flash memory BOOTLOADER_APP_NV_RAM = READ_ONLY 0x01CBC TO 0x1DFF; // Flash memory BOOTLOADER_ZDO_NV_RAM_INIT = READ_ONLY 0x1E00 TO 0x1E95; // Flash memory NVM_ZIGBEE_DATA_SECTION0 = READ_ONLY 0x1E96 TO 0x1FFF; // Flash memory NVM_ZIGBEE_SECTION0_ID = READ_ONLY 0x1FFA TO 0x1FFF; // Flash memory NVM_ZIGBEE_DATA_SECTION1 = READ_ONLY 0x02000 TO 0x21FF; // Flash memory NVM_ZIGBEE_SECTION1_ID = READ_ONLY 0x021FA TO 0x21FF; // Flash memory // 802.15.4/App. flash memory - section 2 APP_CODE_2 = READ_ONLY 0x02200 TO 0xFFAF; // Flash memory RES_NV_REGISTERS_FLASH = READ_ONLY 0xFFB0 TO 0xFFBF; // None-volatile registers RES_IRQ_VECTORS_TABLE_FLASH = READ_ONLY 0xFFC0 TO 0xFFFD; // ISR vectors // Note! 802.15.4/App. does not have its own reset vector. RES_RESET_VECTOR_FLASH = READ_ONLY 0xFFFE TO 0xFFFF; // System reset vectorEND// **************************************************************************// Here it is listed how the variables and code must be allocated.PLACEMENT MY_ZEROPAGE INTO DIRECT_ADDRESSING_MEMORY; DEFAULT_RAM INTO APP_RAM; DEFAULT_ROM INTO APP_CODE,APP_CODE_1, APP_CODE_2; .startData INTO APP_STARTUP_STRUC_FLASH; RST_APP_VARIABLE INTO RST_APP_VAR; CODE_EXECUTION_FROM_RAM INTO CODE_EXECUTION_FROM_RAM0; ZS_NV_RAM_POINTER INTO ZS_NV_RAM_POINTER_RAM; MAC_NV_RAM_POINTER INTO MAC_NV_RAM_POINTER_RAM; NVM_SCRATCHPAD_POINTER INTO NVM_SCRATCHPAD_POINTER_RAM; NVM_SCRATCHPAD_DATA0 INTO NVM_SCRATCHPAD; BOOTLOADER_MAC_NV_DATA0 INTO BOOTLOADER_MAC_NV_RAM; BOOTLOADER_PHY_NV_DATA0 INTO BOOTLOADER_PHY_NV_RAM; BOOTLOADER_APP_NV_DATA0 INTO BOOTLOADER_APP_NV_RAM; BOOTLOADER_ZDO_NV_DATA INTO BOOTLOADER_ZDO_NV_RAM_INIT; NVM_ZIGBEE_DATA0 INTO NVM_ZIGBEE_DATA_SECTION0; NVM_ZIGBEE_DATA0_INIT INTO NVM_ZIGBEE_SECTION0_ID; NVM_ZIGBEE_DATA1 INTO NVM_ZIGBEE_DATA_SECTION1; NVM_ZIGBEE_DATA1_INIT INTO NVM_ZIGBEE_SECTION1_ID; NV_REGISTERS_SECTION INTO RES_NV_REGISTERS_FLASH; SSTACK INTO APP_STACK_RAM; IRQ_VECTOR_SECTION INTO RES_IRQ_VECTORS_TABLE_FLASH;END// **************************************************************************VECTOR 0 _Startup /* reset vector: this is the default entry point for a C/C++ application. *///VECTOR 0 Entry /* reset vector: this is the default entry point for a Assembly application. *///INIT Entry /* for assembly applications: that this is as well the initialization entry point */