I have installed Quickstart 2.7.3 and setup CW 11.1 to launch the GCVT tool.
I have been unable to get the GCT tool to launch from CW 11.1.
I get the following error message when launching GCT:
Variable references empty selection: ${project_loc}
Why would I get this error message about empty selection of ${project_loc}?
I have the GCT tool configured to run externally from CW as: C:\nxp\DSC56800EX_Quick_Start_r2.7\tools\gct\gct56F800.exe
I have Working Dir and Arguments set to: ${project_loc}
Can I run C:\nxp\DSC56800EX_Quick_Start_r2.7\tools\gct\gct56F800.exe as a stand alone executable and pass arguments to the application at runtime?
Thanks for your help with the GCT tool,
Darrell
Hi,
It is complicated to install the QuickStart tools.
Pls download the "DSC56800EX Quick Start User Guide" from the link:
The first part of the "DSC56800EX Quick Start User Guide" is how to install quickstart tools, pls follow up.
Hope it can help you
BR
XiangJun Rong