KINETIS512_SC download problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KINETIS512_SC download problems

2,497 Views
leccy
Contributor III

Trying to download "hello world" RAM project from KINETIS512_SC to TWR-K60N512.

 

Get the following error:

  Launching k60-hello-world_MK60N512VMD100_INTERNAL_RAM_PnE U-MultiLink has encountered a problem.

  Failed to resume target process., Downloading ELF file

 

CW10.1

W7 32bit

 

I noticed that after I had imported the file as described in the documentation accompanying  KINETIS512_SC, I had to create a Remote System connection.

 

Someone point the obvious out to me?!

Labels (1)
0 Kudos
Reply
3 Replies

1,681 Views
dmarks_ls
Senior Contributor II

I don't know what the root cause of your problems may be, but I just encountered the same error message several times ("Failed to resume target process, Downloading ELF file").  It persisted through a project clean/rebuild, power-cycle of target, and power-cycle of workstation.  I was trying to debug a program that I had been successfully downloading and debugging two hours earlier today.

 

It appears that my solution was to create a brand-spanking new project, and flash it to the target.  I got the ominous "secure flash bit" warning or whatever it is, hadn't seen it in a while, but I clicked through and debugged the new app.  I then closed it, re-opened my earlier project, debugged it, and it actually decided to cooperate and download to the target this time.

 

I had earlier tried debugging a bootloader-style application directly, which is probably not allowed.  But that attempt apparently left the target in such a state, that the tools had no idea how to deal with this condition, and just threw up a useless error message.  I'm really getting tired of dealing with beta-quality tools.

1,681 Views
leccy
Contributor III

I ended up raising a query over the KINETIS512_SC_1 demos, and was told to use "CW_MCU_v10_1_Examples" instead...

Beta tools indeed.

 

I also had that security warning when trying AN4379SW bootloader (which to be fair I thought was good).  Turns out that there is an unwanted feature in the IDE which mis-interprets exactly how the security fields can or can't be changed.  Flashing the tower went ok, and continues to work.

0 Kudos
Reply

1,681 Views
dmarks_ls
Senior Contributor II

leccy wrote:

I also had that security warning when trying AN4379SW bootloader (which to be fair I thought was good).  Turns out that there is an unwanted feature in the IDE which mis-interprets exactly how the security fields can or can't be changed.  Flashing the tower went ok, and continues to work.


Regarding the bootloader, you may also want to have a look at this thread:

https://community.freescale.com/message/102662#102662

 

Not the same bootloader you're using, but good to know if you ever try to get the MSC bootloader working.

0 Kudos
Reply