KEA-128 on Eclipse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,047件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    I tried to run KEA-128 on Eclipse.It throwed me this error in arm_end.c.

141027_141027.pngScreenshot (37).png

How to fix this?

ラベル(1)
0 件の賞賛
返信
1 解決策
946件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Vignesh

By default, the head file " ansi_parms.h" locates under:

C:\Freescale\CW MCU v10.6.4\MCU\ARM_GCC_Support\ewl\EWL_C\include

Could you please check whether this path is included in Project Properties?  You can do it from <Project> Menu->Properties, then go to "C/C++ Build-> Settings" panel, then choose "ARM Ltd Windwos GCC C Compiler-> Directories", please check whether the above path is correct. Please see the attached screenshot.

Include Path.png

Hope this helps!

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
947件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Vignesh

By default, the head file " ansi_parms.h" locates under:

C:\Freescale\CW MCU v10.6.4\MCU\ARM_GCC_Support\ewl\EWL_C\include

Could you please check whether this path is included in Project Properties?  You can do it from <Project> Menu->Properties, then go to "C/C++ Build-> Settings" panel, then choose "ARM Ltd Windwos GCC C Compiler-> Directories", please check whether the above path is correct. Please see the attached screenshot.

Include Path.png

Hope this helps!

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信