Issue with Reserved range overlap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with Reserved range overlap

ソリューションへジャンプ
541件の閲覧回数
MWMinor
Contributor V

Hi

 

I have migrated my CW V10.6 tools to a new laptop. When I imported a design (Coldfire MCF51JM128 product design) from my old laptop ( which also was running V10.6) I successfully compiled the design but am failing to programme the devices on my custom board. The board was working with the old laptop, but now I get an error;

58958_58958.pngpastedImage_0.png

I'm not sure where the configuration file is stored/generated, can anyone help me please.

 

Thanks

 

Ken

ラベル(1)
0 件の賞賛
返信
1 解決策
409件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The memory configuration file is usually stored inside <project>\Project_Settings\Debugger\*.mem

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
410件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The memory configuration file is usually stored inside <project>\Project_Settings\Debugger\*.mem

Erich

0 件の賞賛
返信
409件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ken,

from the error screenshot, the error is on the memory configuration file. please refer with attached video to check your memory configuration file setting.

I also attach MCF51JM128.mem from my side.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信