Issue while importing into CW 10.6.4 an old project for CW 7.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue while importing into CW 10.6.4 an old project for CW 7.2

跳至解决方案
1,631 次查看
smanni
Contributor II

Hi, I want to import into CW 10.6.4 an old project for CW 7.2 for the target processor MCF5329.

 

I've used the import wizard: File->Import->CodeWarrior->CodeWarrior Classic Project and after selecting the .mcp project file I get into this error "This toolchain is not supported for this target".

 

145731_145731.pngScreenshot 2016-04-12 16.02.12.png

 

Is there a way to overcome this without creating a new project from scratch? Could you please point out some AN, wiki, tutorial, whatever on how import from CW7.x to CW10.6.x?

 

Thanks.

Regards,

Stefano

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,392 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Stefano

The Project Importer in v10.6.4 only supports DSC products.

For other products, the solution is to create a new bareboard project in CW10.6.4, and then add/copy all your source files to the new project. This is the cleanest way to import a project. Below is an application note for how to do this:
http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

And for Coldfire products, you can also refer to:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4104.pdf

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,393 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Stefano

The Project Importer in v10.6.4 only supports DSC products.

For other products, the solution is to create a new bareboard project in CW10.6.4, and then add/copy all your source files to the new project. This is the cleanest way to import a project. Below is an application note for how to do this:
http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

And for Coldfire products, you can also refer to:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4104.pdf

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复