Is there a place I can download the processor libraries for MPC5668G?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a place I can download the processor libraries for MPC5668G?

1,363件の閲覧回数
andrewdahl
Contributor I

I have downloaded and installed Code Warrior 10.6 from the Freescale site, but when I installed, the installer wasn't able to access the processor specific files because our network proxy would allow it access.  I tried to provide proxy settings and login credentials, but nothing would work.

 

So now I have it installed, but I have no way to compile my project.

 

Is there any place I can download the necessary files and then incorporate them into Code Warrior via some kind of "offline" method?

 

Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,276件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Andrew,

To download the offline installer you must access it via the download page.

pastedImage_0.png

As you can see there are 2 installers:

      Offline one 1.4GB

      Online one 432 MB

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信