Is there a common compiler that runs under eclipse for 9s12 and coldfire that runs on Win7?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there a common compiler that runs under eclipse for 9s12 and coldfire that runs on Win7?

1,106 次查看
nikhilthiruveng
Contributor I

Hi Guys,

I want to know whether there is a common compiler that runs under eclipse, maybe, for 9s12 and ColdFire, that runs on Win7.

Are there compilers other than Codewarrior for 9s12 and Coldfire processors????

Thanks in advance.

N


标签 (1)
0 项奖励
回复
1 回复

980 次查看
dataScout
NXP Employee
NXP Employee

Hello,

ColdFire build tools are integrated in CodeWarrior for MCU 10.x (which is Eclipse based) - this runs on Win7

S12 build tools are not integrated in Eclipse based CW, but the Classic CW (5.1 in S12 case) works under Win7 (but need to be installed under an accessible path (other than Program Files (x86)), or to be run as Administrator)

Regards

0 项奖励
回复