Is Codewarrior for s12(x) V5.1 support the device(MC9S12XEA256)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is Codewarrior for s12(x) V5.1 support the device(MC9S12XEA256)?

跳至解决方案
1,194 次查看
whz
Contributor I

I downloaded CWS5.1 from WWW.NXP.COM, but cann't find the device(MC9S12XEA256) when building project,or when choosing "Project>>change MCU/Connection",Does which codewarrior support MC9S12XEA256? OR Is there a way to add the device?

标签 (1)
0 项奖励
回复
1 解答
1,037 次查看
TICS_Fiona
NXP Employee
NXP Employee

There is no MC9S12XEA256 in the selection list when creating a new project CodeWarrior, however Processor Expert support this device. 

Since the 9S12XEA128/256 are a special bondouts for access to extra ADC channels in 80QFP, and the MC9S12XEA256 is similar to MC9S12XET256-80QFP. User can first create a new project with wizard for MC9S12XET256, selecting Processor Expert at "Rapid Application Development Options".

After create the project with Processor Expert, add the CPU component for MC9S12XEA128_80 to replace MC9S12XET256.

Hope this will help you.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,038 次查看
TICS_Fiona
NXP Employee
NXP Employee

There is no MC9S12XEA256 in the selection list when creating a new project CodeWarrior, however Processor Expert support this device. 

Since the 9S12XEA128/256 are a special bondouts for access to extra ADC channels in 80QFP, and the MC9S12XEA256 is similar to MC9S12XET256-80QFP. User can first create a new project with wizard for MC9S12XET256, selecting Processor Expert at "Rapid Application Development Options".

After create the project with Processor Expert, add the CPU component for MC9S12XEA128_80 to replace MC9S12XET256.

Hope this will help you.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------