Installation error of CW 6.0 for MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Installation error of CW 6.0 for MCU

跳至解决方案
2,211 次查看
shadoooo
Contributor I
Hello!
I'm tring to install Codewarrior 6.0 for MCU I downloaded from the website.
The installer works good until it reaches 0% remaining files, then a Codewarrior IDE appears for a fraction of second and disappears, then the machine hangs-up, just mouse cursor is moving, but application are not more responsive. I'm forced to reset the machine, and after the reboot if I try to start CW it tells me that it isn't installed correctly.
What should I do?
I tried several times with no luck...


Message Edited by shadoooo on 2007-07-18 04:27 PM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,077 次查看
CrasyCat
Specialist III
Hello
 
Which Windows OS are you running on your host?
I would also recommend to remove all Multilink, InDart and other debugging cable from the Host PC before you start installation.
 
If this does not work, you will need a support engineer to look at that.
Please submit a service request for that.

Click here to submit a service request.
Make sure to specify your Host OS in the SR.

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,077 次查看
Curt
Contributor IV
Hi.
Search this forum for your operating system, and see if you turn up any answers.
I've lost track of which versions of windows CW does and does not support. 
 
Might also scan here for threads on installation failures.
 
Regards,
Curt
 


Message Edited by Curt on 2007-07-18 12:05 PM
1,078 次查看
CrasyCat
Specialist III
Hello
 
Which Windows OS are you running on your host?
I would also recommend to remove all Multilink, InDart and other debugging cable from the Host PC before you start installation.
 
If this does not work, you will need a support engineer to look at that.
Please submit a service request for that.

Click here to submit a service request.
Make sure to specify your Host OS in the SR.

CrasyCat
0 项奖励
回复