IO pin status during debug.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IO pin status during debug.

跳至解决方案
1,320 次查看
juliancox
Contributor V

Is it possible to monitor the status of I/O pins in CodeWarrior during a debug session using Multilink? I would like to see the configuration and pin output value (logical, of course) as I single-step through the code. I can measure the actual voltage, but this does not match the value written to the pin register. 

标记 (3)
0 项奖励
回复
1 解答
1,171 次查看
juliancox
Contributor V

Thanks, it answers my question. I am migrating from KEIL IDE (LPC9XX) and they display a peripheral as a graphic in which I can set/clear any bit in any register by clicking on the appropriate box. I guess I was looking for something similar. 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,172 次查看
juliancox
Contributor V

Thanks, it answers my question. I am migrating from KEIL IDE (LPC9XX) and they display a peripheral as a graphic in which I can set/clear any bit in any register by clicking on the appropriate box. I guess I was looking for something similar. 

0 项奖励
回复
1,171 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian,

Yes, you can check the related register on Register view on CW:

pastedImage_1.png

Please enable the "Refresh While Running" , then register can  update in running time .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复