ICS custom trim on CW 6.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ICS custom trim on CW 6.1

ソリューションへジャンプ
2,533件の閲覧回数
fabio
Contributor IV
Hi,

Did anybody noticed any problem with the trim customizing feature of CW6.1?

Using CW6.0 I could set the desired ICS frequency and the NV_FTRIM and NV_ICSTRM were programmed accordingly.

Using CW6.1 I set the desired frequency for the ICS internal reference but it appears that this custom frequency is not read by CW. The debugger/BDM keeps setting the ICS to the default 16MHz operation.

Is this only happening to me?

Best regards,


Message Edited by fabio on 2008-03-14 05:02 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,393件の閲覧回数
J2MEJediMaster
Specialist I
Just got the word back from the engineers and you're right: that feature is broken. The problem has been reported and logged earlier. It will be fixed in the next release. Sorry for the inconvenience.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,393件の閲覧回数
Klined
Contributor I
Hi,

I can say you are not the only one experiencing this.  I have noticed the same behavior when I upgraded from CW 6.0 to 6.1, and I'll say it's quite annoying.  For those situations requiring correct custom trim, I still use CW 6.0.  I hope they fix this in CW 6.1 or the next release.

0 件の賞賛
返信
1,393件の閲覧回数
J2MEJediMaster
Specialist I
I am looking into this.

---Tom
0 件の賞賛
返信
1,394件の閲覧回数
J2MEJediMaster
Specialist I
Just got the word back from the engineers and you're right: that feature is broken. The problem has been reported and logged earlier. It will be fixed in the next release. Sorry for the inconvenience.

---Tom
0 件の賞賛
返信