Is all
Hi,
could you please upload a problem screenshot?
Thanks,
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
This the screenshot
I beginning in Codewarrior, Cyclonepro and have Codewarrior ver. special
5.2 and Cyclonepro Corvus
The microcntroller is 9S12P128 for liquid sensor and scrren 20X4
Alphanumerics
Atte.
Héctor Leal
P.D. I am sorry mi bad english
2018-02-22 7:02 GMT-06:00 ZhangJennie <admin@community.nxp.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: I am using the 9s12p128 and codewarrior ver 5.2, why no load the file
*.abs in debugger with PEmicre corvus ?
reply from ZhangJennie
<https://community.nxp.com/people/ZhangJennie?et=watches.email.thread> in *CodeWarrior
for MCU* - View the full discussion
<https://community.nxp.com/message/989153?commentID=989153&et=watches.email.thread#comment-989153>
Hi Hector
I would suggest you go to debugger menu "File", "Configuration...", force your code stop at a function after load:
Can this help you? If not, please upload your demo project, I have to check it directly.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hector,
I didn't see your project, can you send it?
Thanks.
Jennie Zhang
Hello Jennie:
In this mail is the project 
Project_1.rar
<https://drive.google.com/file/d/1SvbJrB_P0bHNznorXqJWiXNDZpOpKUDW/view?usp=drive_web>
Tanks
2018-02-27 0:28 GMT-06:00 ZhangJennie <admin@community.nxp.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: I am using the 9s12p128 and codewarrior ver 5.2, why no load the file
*.abs in debugger with PEmicre corvus ?
reply from ZhangJennie
<https://community.nxp.com/people/ZhangJennie?et=watches.email.thread> in *CodeWarrior
for MCU* - View the full discussion
<https://community.nxp.com/message/990476?commentID=990476&et=watches.email.thread#comment-990476>