Hi I’m new using codewarrior and the HCS12 T-board, onboard is the mc9s12dp512 chip.
I want to use the timer to count 1 millisecond till a overflow occurs. When a overflow occurs I want to use an interrupt to call a sub routine.
Here is a bit of my code. This interrupt implementation doesn’t work. What am I doing wrong?
void SetTimer(void)
{
TCNT = 0xE0C0;
TSCR1 = 0x90;
}
interrupt 16 void TimerCount(void)
{
ms++; //global variable
TCNT = 0xE0C0;
}
when I built my project I’ll get the following error message.
Link error: L1907: fixup overflow in _Vector_16, TimerCount type 1, at offset 0x0
Could anyone help me with this problem?
Greetings dan23
已解决! 转到解答。