How to program DSP56F805F?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to program DSP56F805F?

623 次查看
khengwahtan
Contributor I


Please help to provide CW software step by step to program .elf file into DSP56F805F.

标签 (1)
0 项奖励
回复
1 回复

577 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello

Do you have CodeWarrior project for the ELF file? If yes, just open the project and click on the ‘debug’ icon to program the target. If you only have ELF file without project, please refer to the section ‘Debugger for 56800E-> Loading .elf File without Project’ in 56800E Targeting Manual:

C:\program files\Freescale\CodeWarrior for DSC56800E v8.3\Help\PDF\Targeting_56800E_cd.pdf

Hope this helps!

 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复