How to generate Half-bridge pwm signals with dead-time using coldfire v1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to generate Half-bridge pwm signals with dead-time using coldfire v1

1,443 Views
diabolostyles
Contributor I

Hello guys,

Is there a way I can generate a half-bridge pwm signals with dead-time using coldfire v1 ?

I'm using the mcf51jm128

I need to generate two complementary pwm signals with a dead-time in between the up and down of each others.

Frequency around 60-100khz would be enough.

It could also be done setting a duty cycle under 50% and being able to delay one pwm from another.

You'll be able to find context schematics attached.

Any help would be great,

Thanks already !

0 Kudos
Reply
1 Reply

1,332 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I am not sure if I got properly your question, but maybe those application note can help you.

https://www.nxp.com/docs/en/application-note/AN3731.pdf 

and

https://www.nxp.com/docs/en/application-note/AN3729.pdf 

Regards

Vicente Gomez

0 Kudos
Reply