How to extract information from the project.abs.s19 file?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to extract information from the project.abs.s19 file?

跳至解决方案
3,718 次查看
thysell
Contributor I
Hi
 
I run a HCS08 and am using CW5.0.
 
My setup is that I have an application and a bootloader, these seem to work allright. What I wonder now is how to extract the relevant information from the project.abs.s19 file? How do I parse it so that I know which bytes are the interruptvectors and which bytes are the application and so on.
 
I want to do this because my Flash is divided into three sections... One large that contains the application, the second is a small one that contains the bootloader and the third one is as big as the first one... I want to transfer a new application to this last section... But the problem is what to send to this section? The project.abs.s19 file seems to bee to large... so I wonder how to parse it into the different parts of the program...
 
Is this doable?
 
thank you
 
//Thysell
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,091 次查看
Alban
Senior Contributor II
Hello,
 
This is not only doable, but already done.
If you search for "S-Record format" you will see quite a few documentation explaining how to extract info from the the S19. www.s-record.com is ONE example of good resource.
All info you need is IN CLEAR in the S19.
 
Also, you can see some Application Notes called bootloaders which re-program the Flash on-board, by receiving an S-Record via a serial port (CAN, SCI, SPI).
 
Cheers,
Alban.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,092 次查看
Alban
Senior Contributor II
Hello,
 
This is not only doable, but already done.
If you search for "S-Record format" you will see quite a few documentation explaining how to extract info from the the S19. www.s-record.com is ONE example of good resource.
All info you need is IN CLEAR in the S19.
 
Also, you can see some Application Notes called bootloaders which re-program the Flash on-board, by receiving an S-Record via a serial port (CAN, SCI, SPI).
 
Cheers,
Alban.
0 项奖励
回复
2,091 次查看
thysell
Contributor I
sweet!
 
I'll check it out... probably not until monday though... I'm in sweden and its almost time to go have a beer...
 
thank you
 
//thysell
0 项奖励
回复