I will answer myself. The answer is found in S12X Examples.pdf.
1) Add #pragma statements in the source code that tell the compiler how to access these
variables and under what name (segment name) these variables can be referred to by the
linker:
a) #pragma DATA_SEG __GPAGE_SEG GLOBAL_RAM
and/or
b) #pragma CONST_SEG __GPAGE_SEG GLOBAL_FLASH
2) In the linker parameter file (extension .prm), place this segment into the correct
memory ranges.
a)
PLACEMENT
...
PAGED RAM_0F_GLOBAL = READ_WRITE 0x0F8000'G TO 0x0FBFFFF'G;
/* 16 kByte global address range covering RAM_F8 .. RAM_FB */
...
END
b)
PLACEMENT
...
FLASH_7E_GLOBAL=READ_ONLY 0x7E0000'G TO 0x7EFFFF'G;
/* 64 kByte global address range covering PAGE_F8..PAGE_FB */
...
END
Note: Make sure to delete of comment the corresponding definitions for the banks that
overlap this global addresses!
3) make sure to specify the option -D__FAR_DATA on the compiler command line. This
will enable the correct initialization in the startup code.
4) any pointer pointing to global data needs to be qualified with “__far”:
c
har *__far myPtr;