How to add an include file to inline assembly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add an include file to inline assembly

ソリューションへジャンプ
1,628件の閲覧回数
snickface
Contributor I

I want to use inline assembly, within a 'C' environment to implement some functions. I need to add an "include file" so that I don't get undefined errors. How do I include an "include file" in inline assembly? I'm using CodeWarrior 10.2 for microcontrollers and an MC12311CHN chip which contains an HCS08 microcontroller.

Example:

void foo (void)

{

  asm

  {

sta FCMD ; command the flash

  }

}

Without an include file such as mc9s08qe32.inc, FCMD is undefined.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,377件の閲覧回数
bigmac
Specialist III

Hello, and welcome to the forum.

 

For a .c file that references any hardware registers, you should

#include "derivative.h"

 

or alternatively

#include <mc9s08qe32.h>

 

The first file is created by the project wizard, and references the header file for the device.  For the second method, you are doing this directly.  The first method is preferred - should you ever change the device used for a project, derivative.h will be automatically updated by the wizard.

 

There is a macro for FCMD within the device header file.

 

Regards,

Mac

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,378件の閲覧回数
bigmac
Specialist III

Hello, and welcome to the forum.

 

For a .c file that references any hardware registers, you should

#include "derivative.h"

 

or alternatively

#include <mc9s08qe32.h>

 

The first file is created by the project wizard, and references the header file for the device.  For the second method, you are doing this directly.  The first method is preferred - should you ever change the device used for a project, derivative.h will be automatically updated by the wizard.

 

There is a macro for FCMD within the device header file.

 

Regards,

Mac

 

0 件の賞賛
返信