MCU:mc9s08jm16
in bootlaoder code I define: unsigned char v1 @0x1880
in other source code file I define: unsigned char V2 @0x1880
when i buld the poject, there are errors: Segments .absSeg11(0x1880) and .absSeg22(0x1880) overlap.
How to fix this error?
I have to define two different name point to 0x1880.
解決済! 解決策の投稿を見る。
Hello,
you have several options:
a) disable linker message
add -WmsgSd1100 to your linker options
b) use defines like this
#define VAR_ADDRESS 0x1880unsigned char var @VAR_ADDRESS;#define v1 (*((unsigned char*)VAR_ADDRESS))#define v2 (*((unsigned char*)VAR_ADDRESS))
hope this helps,
BK
I am using CW10.0
Hello,
you have several options:
a) disable linker message
add -WmsgSd1100 to your linker options
b) use defines like this
#define VAR_ADDRESS 0x1880unsigned char var @VAR_ADDRESS;#define v1 (*((unsigned char*)VAR_ADDRESS))#define v2 (*((unsigned char*)VAR_ADDRESS))
hope this helps,
BK
Hello,
Another possibility may be to define v2 as an alias for v1, within the file that uses v2. Personally, I do not like to disable error messages that may hide an important coding error elsewhere in the code.
#define v2 v1 // v2 is an alias for v1
Regards,
Mac
I am so appreciate your repay. Thank you very much.
could you please kindle provide more information about :
"a) disable linker message
add -WmsgSd1100 to your linker options"
I am a new hand in using CW. I don't know how to "disable linker message" .
is it a option in the CW setting? or I have to add -WmsgSd1100 into my source?
Please please tell me the detail steps to disable the linker message. Thanks a lot.
Hello,
sure thing.
Select the project, then use the menu Project > Properties.
Then see attached screenshot.
Hope this helps,
BK
PS: Screenshot is from MCU10.2. MCU10.0 is really old, I suggest that you are using 10.2 instead. But options should be the same.
Hello,
Thanks for your patient reply.
I am using CW10.0. And my setting interface is different from yours.
Please help to check if the setting is correct. (see the attached pic)
I check the" disable user message" and add the "WmsgSd1100" into the rectangle.
Another question: I click "check update" and a pop dialoge said:' There are no update sites to search. Do you wish to open the "Available Software Sites" preferences.
Hello,
about the linker option: add it to the 'other flags' in MCU10 prior 10.2 (see attached screenshot).
BK
Hello.
Does it mean I have to add -WmsgSD1100 to two places?
(1) Poject -> Properties -> C/C++Build ->Setting -> Message: check Disable user message, add -WmsgSD1100 into other falg rectangle.
(2) Poject -> Properties -> C/C++Build ->Setting -> Linker -> General -> add -WmsgSD1100 into other falg rectangle.
more question: I found there is a "-WmsgFob"%f%e:%l:%k..."exist the "other falg rectangle"
what's that ? Can i delete it ?
Hello,
add it only once, into the linker settings.
And keep the other options like "-WmsgFob"%f%e:%l:%k..." (this one formats the error messages, see the description in the manual).
BK
ok. Got it....
I can't thank you more.
Have a nice weekend...
Hello,
on upgrading to 10.2:
You cannot upgrade from 10.0 to 10.x from within eclipse/CodeWarrior.
The update you tried only applies for service packs and fixes.
To get MCU10.2 you need to download it from here:
http://www.freescale.com/cwmcu10
You still can keep your current installation (no need to uninstall).
Hope this helps,
BK