How to Fuse my application in KwikStik k40

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Fuse my application in KwikStik k40

860件の閲覧回数
yasararafath
Contributor II

I have completed my application and found running fine from codewarrior IDE into the Kwikstik k40. But once when I remove or power of the board the application is not running.

 

Now I want to port it permanently to the Kwikstik k40 board.

 

What to do?

 

Anyone please.........

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

738件の閲覧回数
yasararafath
Contributor II

THank you for your information friend. I did the same before (Clean, rebuild and downloaded it.). But in power on reset the application is not running, once again I have to debug the same thru codewarrior IDE. If u have any solution pls reply me soon.

0 件の賞賛
返信

738件の閲覧回数
JimDon
Senior Contributor III

Are you using the FLASH build? The RAM build will obviously not run after a reset.

On the "Project/Build configurations/Set active" menu, hopefully there is a Flash build of the project.

Clean, rebuild and download it.

0 件の賞賛
返信