How do I disable the "Always Erase and Program flash without asking" option in the Hardware Connection Advanced Programming Options?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I disable the "Always Erase and Program flash without asking" option in the Hardware Connection Advanced Programming Options?

1,525 Views
mjosborne
Contributor II

Hello,

 

this is a re-post of Re: How do I disable the "Always Erase and Program flash without asking" option in the Hardware Conn... There is a separate issue around software breakpoints that is being addressed by our FAE; however, we would like to figure this out as it adds a lot of time when debugging...

 

So, in a CodeWarrior10.6 project, when we download our image to external RAM for debugging CodeWarrior always attempts to write to flash. This takes a long time to time-out and fail; we cannot disable this option. Help!

32812_32812.pngAdvanced_Programming_Options.png

Labels (1)
0 Kudos
Reply
1 Reply

1,307 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Matt,

Apologies for the delayed response, I have just received confirmation from P&E that there is no way to disable the "Always Erase and Program flash without asking" option.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply