How can i build S19 file in CodeWarror for HCS12(X) 5.1 Special version?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i build S19 file in CodeWarror for HCS12(X) 5.1 Special version?

ソリューションへジャンプ
1,845件の閲覧回数
kernwang
Contributor II

Due to the code is less than 4K, i do not buy a license for CW.

How can i build S19/Hex file in CodeWarror for HCS12(X) 5.1 Special version?

Or could you please help to show a training document ?

Thanks!

ラベル(1)
1 解決策
1,544件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

The C code and data size is restricted to 32 KB in Special Edition of CW5.1.

An S19 file should automatically be generated if your project includes a file with extension *.bbl that contains instructions to let the burner utility know how to generate this s19 file.  This file is normally located under your project's bin folder.

If you are not seeing this file in your project, please check that you have a *.bbl file. You can generate such a file by doing the following :

1) Press ALT +F7

2) Click on Burner for HC12

3) Click on the "Burner" button

4) Click on the "Content" tab - Make sure the Motorola S Format is selected

5) Switch to the "Command File" tab. Copy  the contents that appear on this window and paste them into a regular text file. Name this file as "burner.bbl" and save it into your project folder. Add this file to your project. 

This should let CodeWarrior generate a .s19 file upon a successful build.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,545件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

The C code and data size is restricted to 32 KB in Special Edition of CW5.1.

An S19 file should automatically be generated if your project includes a file with extension *.bbl that contains instructions to let the burner utility know how to generate this s19 file.  This file is normally located under your project's bin folder.

If you are not seeing this file in your project, please check that you have a *.bbl file. You can generate such a file by doing the following :

1) Press ALT +F7

2) Click on Burner for HC12

3) Click on the "Burner" button

4) Click on the "Content" tab - Make sure the Motorola S Format is selected

5) Switch to the "Command File" tab. Copy  the contents that appear on this window and paste them into a regular text file. Name this file as "burner.bbl" and save it into your project folder. Add this file to your project. 

This should let CodeWarrior generate a .s19 file upon a successful build.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,544件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kern,

After you build your project , you can find the  S19 file under the project -> bin .

For example :

..\Project_8\bin\Project.abs.s19

Hope it helps

Alice

0 件の賞賛
返信