The C code and data size is restricted to 32 KB in Special Edition of CW5.1.
An S19 file should automatically be generated if your project includes a file with extension *.bbl that contains instructions to let the burner utility know how to generate this s19 file. This file is normally located under your project's bin folder.
If you are not seeing this file in your project, please check that you have a *.bbl file. You can generate such a file by doing the following :
1) Press ALT +F7
2) Click on Burner for HC12
3) Click on the "Burner" button
4) Click on the "Content" tab - Make sure the Motorola S Format is selected
5) Switch to the "Command File" tab. Copy the contents that appear on this window and paste them into a regular text file. Name this file as "burner.bbl" and save it into your project folder. Add this file to your project.
This should let CodeWarrior generate a .s19 file upon a successful build.
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------