Hi Oleg,
With CW for DSP v8.3 and previous version Processor Expert (PEx) feature was included.
PEx includes a bean to manage the Flash memory in your application.
This bean is named IntFLASH.
You will find more details at installation folder:
\CodeWarrior for DSC56800E v8.3\ProcessorExpert\BEANs\IntFLASH
You can create an example using the bean too with the project wizard:
File + New .. + Processor Expert Examples Stationery + DemoApplications + HWBeans + 56F80x + InFlash
The Example is for DSP56F807 but you can move to 803.
To do that you just need to add a the DSP56F803 device and select it.
The Generated code will be done for DSP56f803.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------