Hiwave.exe caught in infinite loop

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hiwave.exe caught in infinite loop

跳至解决方案
3,503 次查看
pittbull
Contributor III
Hello,

I'm using CodeWarrior for HCS12X version 4.1. I copied a project from one computer to another. When I try to run the debugger on this project, it hangs in an infinite loop - the command output shows 'ADDXPR numbytes' repeatedly.

I think there is something in an .INI or CMD file that I must delete. How can I get rid of that?

Thanks in advance,
pittbill
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,528 次查看
CrasyCat
Specialist III

Hello

Can you check in the directory where the .abs file is located (usually this is the{Project}\bin directory).

You probably have a file with extension .xpr there.

In order to avoid the loop, close the debugger and delete the .xpr file.

This should do it.

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,529 次查看
CrasyCat
Specialist III

Hello

Can you check in the directory where the .abs file is located (usually this is the{Project}\bin directory).

You probably have a file with extension .xpr there.

In order to avoid the loop, close the debugger and delete the .xpr file.

This should do it.

CrasyCat

0 项奖励
回复
1,528 次查看
pittbull
Contributor III
>> delete the .xpr file.

Thank you, that was it.
0 项奖励
回复