HiWave Assembly windows empty

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HiWave Assembly windows empty

跳至解决方案
2,098 次查看
sebasira
Senior Contributor I

Hi all!

 

I'm using HiWave from CW 3.1.

This is a problem that I'm having since forever, and I think maybe you can help me.

I'd like to know how to display assembly code, so debugging would be easier. Sometimes, I mean for some files or routines, code is shown. But with others (most of) that windows is empty.

 

Should I generate a special output? I'm generating listing file.

 

Thanks!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,839 次查看
CrasyCat
Specialist III

Hello

 

Something strange seems to happen on your system.

 

I would recommend you to submit a service request  for that to get one of our support engineer looking into that
Click here to submit a service request..
 
Make sure to attach  a project reproducing the issue and installed product information to the SR.
To make sure you provide all necessary project information, you can use the Pack and Go wizard.
  - Start the IDE
  - Open the Project
  - Select Help -> "Pack and Go"
  - Follow the instruction on the screen. That will generate a zip file containing all necessary
    information (including the installed product information).

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,839 次查看
CrasyCat
Specialist III

Hello

 

Are you having problems with ANSI C source files or with Assembly source files?

 

Are you generating debug information for the source files?

 

Are you seeing Source code in the Source window?

 

CrasyCat

0 项奖励
回复
1,839 次查看
sebasira
Senior Contributor I

 

Hi CrasyCat!

 

> Are you having problems with ANSI C source files or with Assembly source files?

The trouble is with ANSI C files.

 

>Are you seeing Source code in the Source window?

Yes, I can see the C source file, and I can debug it. But sometimes I need to debug viewing the ASM code executed and the Assembly windows is empty.

 

>Are you generating debug information for the source files?

I guess so... Because I can debug the code, but as I said before, sometimes it would be great if I can see the ASM instruction that it is executing. Now, When I want to know that, I need to go outisde the debugger and take a look at the associated .lst file and look for the line that I was debugging

 


0 项奖励
回复
1,839 次查看
CrasyCat
Specialist III

Hello

 

Did you open an Assembly Component inside of HI-WAVE (Use Component > Open to open a new one)?

 

The purpose of this component is to show disassembly code start at current PC.

The code is disassembled directly from memory.

 

CrasyCat

0 项奖励
回复
1,839 次查看
sebasira
Senior Contributor I

Yes I do. I already have an Assembly component and also try opening a new one. Look the attached files, for exmple, the _Startup has the ASM but my code doesn't

0 项奖励
回复
1,840 次查看
CrasyCat
Specialist III

Hello

 

Something strange seems to happen on your system.

 

I would recommend you to submit a service request  for that to get one of our support engineer looking into that
Click here to submit a service request..
 
Make sure to attach  a project reproducing the issue and installed product information to the SR.
To make sure you provide all necessary project information, you can use the Pack and Go wizard.
  - Start the IDE
  - Open the Project
  - Select Help -> "Pack and Go"
  - Follow the instruction on the screen. That will generate a zip file containing all necessary
    information (including the installed product information).

 

CrasyCat

0 项奖励
回复
1,839 次查看
sebasira
Senior Contributor I

Thanks CrasyCat, I'll do as you said

0 项奖励
回复