I am facing problem of toolchain and build tool. Also please give me the way to import and to build the CW Classic v6.3 project in CW v10.6 ..
Thanks in advance
Hi Xin,
Thanks for your reply.
I am using Coldfire Compiler. And for it I have added tghe source paths for all the source folders.
But still I am facing some error like missing / expected ";" or "(" etc.
could you please help me to figure out the issues?
Thanks in advance
Hello Harshit
CodeWarrior v6.3 for Coldfire is an old version, it could be more easy to move to the v7.2 and be sure the application is running on the last classic version before to move onto Eclipse.
This link should be helpful to you:
https://community.freescale.com/thread/379597
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Harn,
What about your chip ?
Does this thread can help you :
CodeWarrior 6.3 import error .
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice. Could you please Help how to add paths and symbols in C/C++ General in properties of project,
Which files should be added in which tab?
Thanks and regards..
Harshit
Hello Harshit
To import a Classic CodeWarrior Project to Eclipse CW, user needs to create a new bareboard project in CW10.6 and then add/copy all your source files to the new project. This is the cleanest way to import a project. Below is an application not for how to do this:
http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf
In Eclipse CodeWarrior, user can also set the search path for head files and libraries. For head files, please set its search path from <Project> Menu->Properties, then go to “C/C++ Build”-> Settings -> HSC08 Compiler-> Input.
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------