Help, NEW to Codewarrior IDE S12 V5.0 and KIT33812ECUEVME

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help, NEW to Codewarrior IDE S12 V5.0 and KIT33812ECUEVME

1,972 Views
MBEMotorsportsi
Contributor I

Hi am I new to forums, codewarrior and Freescale. I bought the reference design KIT33812ECUEVME a few weeks ago and still havn't been able to do anything with it. How or where do I start. I made all the connections but don't know if I the software has been uploaded or not in the ECU.

I read all the documents but seems to be missing details. Does anyone have detailed step by step instructions on how to get started with the small engine software example?

 

Thanks for all you help 

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

1,165 Views
usmanjavaid
Contributor II

u must start with the spin bench setup

.

after u r certain that the reluctance sensor is giving output u desired than make the wiring connections

.

then edit the software example inn the CD

.

Edit the application definition file to define your engine specs and the size of the lookup tables

.

then edit application map accordin to the specs of your fuel pump and fuel injector you are willing to use

.

u may Contact me via email

usman_fr2@yahoo.com

.

i am working on the same thing nowadays

0 Kudos
Reply

1,165 Views
sammaxel
Contributor I

Hi Usman,

I have just started this KIT33812ECUEVME project.

I have problems: no output signals on Injection and coil output.

are you really ever successfully using this kit on any motorcycle?

thanks in advance

0 Kudos
Reply

1,165 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Alex,

in this link you may find all the getting started documents and software that you may need for this kit. KIT33812ECUEVME: Small Engine Control Reference Design featuring the 33812 and the S12P Product Summ...

in this page you will find a section called Jump Start Your Design in this section you will find the following data:

Let me know if you need more information reading this kit.

Regards,


0 Kudos
Reply

1,165 Views
J2MEJediMaster
Specialist I

Usually the kits come with a Quick Start guide that goes through the set up, stey-by-step. They also (but not always), tell you how the cable the gear up. Did you not find a Quick Start Guide?

 

---Tom

0 Kudos
Reply

1,165 Views
usmanjavaid
Contributor II

hi !

can u tell what might be the problem

.

i am using KIT33812ECUEVME with 8m1 toothed flywheel

.

the output pulses for fuel injector are comming in millivolts there are no high side pullup resistors with these output pins

.

is this pulse whose amplitude is in millivots capable of turning the fuel injector "ON" ---????????????????

.

regards:

Usman

usman_fr2@yahoo.com

0 Kudos
Reply