Has anyone connected the FRDM-KL25Z to Android yet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Has anyone connected the FRDM-KL25Z to Android yet?

跳至解决方案
1,208 次查看
injunear1
Contributor IV

I am planning on using an Android tablet to communicate with Freedom boards. Has anyone figured this out yet?

 

I have been able to do it with two other USB devices. But I need more remote functionality, which is why I selected the Freedom board in the first place. I think it will be great for what I have in mind.

 

But having just gotten my CW IDE working with the board, I haven't gotten to the the Android connectivity yet.

 

I am just wondering if anyone has gotten that far yet.

 

Thank you once again.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
920 次查看
injunear1
Contributor IV

Yes it is possible. I have it working now with a lot of help from the following webpage:

ksksue/FTDriver · GitHub

在原帖中查看解决方案

0 项奖励
回复
1 回复
921 次查看
injunear1
Contributor IV

Yes it is possible. I have it working now with a lot of help from the following webpage:

ksksue/FTDriver · GitHub

0 项奖励
回复