Has anyone connected the FRDM-KL25Z to Android yet?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has anyone connected the FRDM-KL25Z to Android yet?

ソリューションへジャンプ
1,251件の閲覧回数
injunear1
Contributor IV

I am planning on using an Android tablet to communicate with Freedom boards. Has anyone figured this out yet?

 

I have been able to do it with two other USB devices. But I need more remote functionality, which is why I selected the Freedom board in the first place. I think it will be great for what I have in mind.

 

But having just gotten my CW IDE working with the board, I haven't gotten to the the Android connectivity yet.

 

I am just wondering if anyone has gotten that far yet.

 

Thank you once again.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
963件の閲覧回数
injunear1
Contributor IV

Yes it is possible. I have it working now with a lot of help from the following webpage:

ksksue/FTDriver · GitHub

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
964件の閲覧回数
injunear1
Contributor IV

Yes it is possible. I have it working now with a lot of help from the following webpage:

ksksue/FTDriver · GitHub

0 件の賞賛
返信