HCS12 v3.1 debugger limited to assembly step, something happened

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS12 v3.1 debugger limited to assembly step, something happened

ソリューションへジャンプ
2,975件の閲覧回数
borisyost
Contributor II
I have a HCS12 v3.1 system with P&E that used to work fine.  Then I took my code and did debugging and integration at a customer site (with another HCS12 and P&E system).  Now I brought it back, and the debugger doesn't work any more.  It just crashes when you hit F5.  Assembly step still works, though.  So does another engineer's project, and my code from before I left.  And just running (without debugger).  An error message that regularly comes up is 'Can't set breakpont at <...address...>' or something like that, if you try to run-to-cursor or set a breakpoint.
 
Unfortunately, it is simply not practical to gradually roll back what I did on my trip--I changed a lot of stuff, and it would take days.
 
Anybody have any clues?
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
968件の閲覧回数
borisyost
Contributor II

I got it.  I deleted P&E_ICD.ini from the project and copied one from an old project.  Now if I could just have Friday back....

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
969件の閲覧回数
borisyost
Contributor II

I got it.  I deleted P&E_ICD.ini from the project and copied one from an old project.  Now if I could just have Friday back....

 

0 件の賞賛
返信