HCS12 v3.1 debugger limited to assembly step, something happened

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HCS12 v3.1 debugger limited to assembly step, something happened

跳至解决方案
2,974 次查看
borisyost
Contributor II
I have a HCS12 v3.1 system with P&E that used to work fine.  Then I took my code and did debugging and integration at a customer site (with another HCS12 and P&E system).  Now I brought it back, and the debugger doesn't work any more.  It just crashes when you hit F5.  Assembly step still works, though.  So does another engineer's project, and my code from before I left.  And just running (without debugger).  An error message that regularly comes up is 'Can't set breakpont at <...address...>' or something like that, if you try to run-to-cursor or set a breakpoint.
 
Unfortunately, it is simply not practical to gradually roll back what I did on my trip--I changed a lot of stuff, and it would take days.
 
Anybody have any clues?
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
967 次查看
borisyost
Contributor II

I got it.  I deleted P&E_ICD.ini from the project and copied one from an old project.  Now if I could just have Friday back....

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
968 次查看
borisyost
Contributor II

I got it.  I deleted P&E_ICD.ini from the project and copied one from an old project.  Now if I could just have Friday back....

 

0 项奖励
回复