HC08 with CW 5.1 - Digital I/O Hardware Beans

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HC08 with CW 5.1 - Digital I/O Hardware Beans

ソリューションへジャンプ
1,640件の閲覧回数
Joxer
Contributor I
I am using HC08 with CW 5.1 and would like to use the PE to create a bean for some optional hardware on my development board. I have added 4 digital inputs and 4 digital outputs to the development board and I am curious as to which bean to add to my project.
 
I am guessing that it is similar to using the bean for the LEDs on the board but do not know which port type to use in the bean.
 
Thank you for the help.
 
--
Alban Edit: mention product in subject line

Message Edited by Alban on 2007-03-20 05:46 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
970件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
Processor Expert has a tool that you could use for that: Bean Wizard.
The Bean Wizard™ is the tool that allows you to create your own beans that address the specific needs of an application, like the support of using a generic peripheral in a very specific way.
This is included in the Professional Edition only.

In your case , may be you can use on of the Port I/O Beans.
Some other beans are available (free) on the Processor Expert Web site:
http://www.processorexpert.com/

Hope this will help you.
Pascal

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
971件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
Processor Expert has a tool that you could use for that: Bean Wizard.
The Bean Wizard™ is the tool that allows you to create your own beans that address the specific needs of an application, like the support of using a generic peripheral in a very specific way.
This is included in the Professional Edition only.

In your case , may be you can use on of the Port I/O Beans.
Some other beans are available (free) on the Processor Expert Web site:
http://www.processorexpert.com/

Hope this will help you.
Pascal

0 件の賞賛
返信