Hello,
I'm developing on the S912ZVML12 using codewarrior. Is there any possibility to force alignment for a variable.
Something linke this:
volatile uint8 SomeArray[6][4] __attribute__((aligned (4)));
With this line of code the Compiler writes:
"volatile uint8 SomeArray[6][4] __attribute__((aligned (4))) => illegal or unsupported __attribute__"
How can the 32bit alignment forced for this Array?
Thanks
已解决! 转到解答。
Hello Markus,
This feature has been added into the latest relase CodeWarrior for MCU v10.6.
You can download it here:
Stan
Hello Markus,
This feature has been added into the latest relase CodeWarrior for MCU v10.6.
You can download it here:
Stan
Hello Stanislav,
I´m having alignment problems too and I wonder how can I apply the __attribute__((aligned())) in my case:
- I have a struct (let´s call it strSType) with several fields with varying sizes (char F1[11], word F2[2], char F3, dword F4...)
- I read a byte array from memory (let´s say flash) and I want to cast this array so that I can access it by field:
byte by[512];
strSType *pstr;
ReadFromFlash(by,512);
pstr=(strSType *)by;
.... And the use
pstr->F1[]...
pstr->F4...
Any suggestion?
Thanks in advance
Hello Carlos,
If your strSType struct located in flash is initialized by the code in your project e.g.:
const strSType struct_in_Flash = { "hello", {0,1},'1',0x1234....}
then you don't have to consider any padding bytes/alignments within the structure.
But you should possibly consider alignment of byte array by[512] if you require better speed performance.
What kind of problem do you observe? Can you please describe it more in the detail?
Regards,
Stan
Hello Stan,
thanks for the answer.
I´m trying to read data from an external flash memory and process it (for example, reading the master boot record of a FAT filesystem). As I read an array of bytes (let´s call it byArr[512]) without padding bytes but my structure has padding bytes I cannot simply cast the byte array to my struct and expect that each field is located where it should.
For example, I read the 512 bytes of the master boot record of the FAT, and try to cast this byte array to the structure:
typedef struct _MasterBoot_Entries
{
UINT8 ExcecutableCode[446];
Partition_Entries Partitions[4];
UINT16 MBRSignature;
}MasterBoot_Entries;
It happens that ((MasterBoot_Entries *)byArr)->MBRSignature does not match the real value, which is *((UINT16 *)&byArr[510]).
It happens the same with all the fields in each ((MasterBoot_Entries *)byArr)->Partitions[x], as ((MasterBoot_Entries *)byArr)->Partitions is dword aligned, with padding byte before it
Am I missing something?
Regards
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools or 16-bit Microcontrollers ) to get it visible for active members.
For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )
Thank you for using Freescale Community.