Getting CW10 to output S3 (32 bit address) instead of S1 (16 bit address)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting CW10 to output S3 (32 bit address) instead of S1 (16 bit address)

ソリューションへジャンプ
1,448件の閲覧回数
CarlFST60L
Senior Contributor II

Hi,

 

In short, can we get the SREC output (.s19) using CW10 project using RS08SH8 to output S3 instead of S1?

 

We have developed some software tools to remotely update firmware on ColdfireV2 processors (52259), this tool chain requires S3 records. We also have a couple 8 bit processors (RS08SH8) connected which we can update remotely, however, the V2 processor is setup to parse / manage only S3 (32 bit address) files. Is there a converter available to convert S1 to S3, or, can we tell CW10 to output S3 when compiling our 8 bit projects?

 

Thanks,

Carl

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,002件の閲覧回数
CarlFST60L
Senior Contributor II

the solution is to change the burner.bbl line"SRECORD=Sx" to "SRECORD=S3"

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,003件の閲覧回数
CarlFST60L
Senior Contributor II

the solution is to change the burner.bbl line"SRECORD=Sx" to "SRECORD=S3"

0 件の賞賛
返信