Freescale Codewarrior 5.9.0 build 2330 upgrade for QE8 MCU's

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale Codewarrior 5.9.0 build 2330 upgrade for QE8 MCU's

Jump to solution
5,198 Views
BooleanBob
Contributor IV
Hello friends. I am using this compiler that came with my evaluation board. I can make projects for QE128, QE64 and QE96, but I don't have support for QE8's. I already visited the Freescale's 8 bit micrcontroller website for an upgrade but I can't find it. If I try to upgrade my version directly from the software via internet, it seems that there is nothing to upgrade.

Any ideas ?

Thank you in advance.

BooleanBob
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,719 Views
BooleanBob
Contributor IV
stansih, thank you again.
I have installed the 6.2 version and now the QE8 support appears as it should.
Problem solved.
I am sorry that I didn't know that the complete compiler could be downloaded this way.

Greetings from Buenos Aires, Argentina.

BooleanBob

View solution in original post

0 Kudos
Reply
6 Replies
1,719 Views
J2MEJediMaster
Specialist I
The version number you provided is for the CodeWarrior IDE. To get the actual tool version number, choose Help > About Freescale CodeWarrior > Installed Products.

Sometimes you actually have to download a patch file to get support for certain MCU families.

---Tom
0 Kudos
Reply
1,719 Views
BooleanBob
Contributor IV
Thank you Tom.
I could obtain the text file containing what I have actually installed and I attached it.
I can't really tell wich is the compiler file, maybe you can help me.
The question is if there is an update for QE8 and where to obtain it.

Kind regards

BooleanBob

0 Kudos
Reply
1,719 Views
stanish
NXP Employee
NXP Employee
Hi BooleanBob,

I'd strongly recommend you to install the most recent release of CodeWarrior for MCUs v6.2 (Special Edition) and Compiler Patch v6.2.1. This verison fixes several defects and supports recent MCU derivatives.

CodeWarrior v6.2:
http://www.freescale.com/lgfiles/devsuites/HC08/CW_MCU_V6_2_SE_11262008.exe

Compiler Patch v6.2.1:

https://www.freescale.com/webapp/Download?colCode=MCU-V6-2-1-CP&nodeId=0127260061788213CF49A4&appTyp...

There are also several patches that could be installed in order to support additional derivatives.
See the current list of available patches for v6.2:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF49A4


If you insist on using older CodeWarrior release v6.0 I'd suggest you to install all the updates for v6.0 available here:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF26AD



Stanish
0 Kudos
Reply
1,719 Views
BooleanBob
Contributor IV
Thank you stanish.
The compiler that I am using is the one that came in the box of my DEMOQE box that I bought one month ago from our local Arrow Electronics branch in Buenos Aires. I didn't know that one could download a tool without buying a demo kit. By that time, the QE8 existed, so I don't understand why it wasn't provided. So I will try your suggestion.

Cheers

BooleanBob
0 Kudos
Reply
1,719 Views
stanish
NXP Employee
NXP Employee
BooleanBob,

In fact my CW v6.0 offers QE8 derivative in the project wizard. I'm not sure if it's supported due to the fact I've installed several Service Packs (including SP QE128) or if it's already supported by clean V6.0 installation.
Anyway, I'd suggest you to install v6.2 + patches & SPs.

Stanish
0 Kudos
Reply
1,720 Views
BooleanBob
Contributor IV
stansih, thank you again.
I have installed the 6.2 version and now the QE8 support appears as it should.
Problem solved.
I am sorry that I didn't know that the complete compiler could be downloaded this way.

Greetings from Buenos Aires, Argentina.

BooleanBob
0 Kudos
Reply