Flash device,blank check and verify are failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash device,blank check and verify are failed

Jump to solution
4,138 Views
lixinhua
Contributor I

Dear Sir ;

I'm using "MCF5272+ S29JL032J " with CodeWarrior 7.2 to develop a new product . I can't find the ARM in list of the Flash Device , and have to choice S29GL032 as substitution .I can program the MCF5272 , but we are  runuing "blank check" and "verify" are failed . Could you help us to find the root cause ? what are troubel for me to choice "flash device " ?

 

Best Regards ;

 

Tim

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,737 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tim,

If the memory you are using is not listed as part of the supported flash devices you can follow the Application Note AN3390 that explains how to add a new flash device, the document can be found on this path:

C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\Help\PDF\AddFlashDevs.pdf

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

View solution in original post

0 Kudos
Reply
1 Reply
3,738 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tim,

If the memory you are using is not listed as part of the supported flash devices you can follow the Application Note AN3390 that explains how to add a new flash device, the document can be found on this path:

C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\Help\PDF\AddFlashDevs.pdf

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply