Failed to resume target process. Downloading binary to target...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to resume target process. Downloading binary to target...

3,642 Views
guilongxiao
Contributor I

Hello,everyone.I met a problem, urged to solve it.

I run the simple demo in a 52259 development board with CW10.6.

When I run the demo,the cw displays "Failed to resume target process. Downloading binary to target...".

Labels (1)
Tags (2)
0 Kudos
Reply
8 Replies

2,945 Views
BlackNight
NXP Employee
NXP Employee

What that message means is that the debugger is not able to stop and run the processor.

Multiple reasons:

- wrong cpu selected?

- overlapping memory areas? (http://mcuoneclipse.com/2012/03/30/problem-occurred-flash-programming-with-overlapping-memory/)

- wrong debugger connection settings? (Using the FRDM-K64F with CodeWarrior | MCU on Eclipse)

Does it happen as well with the wizard project created by CodeWarrior? then you might have a board problem.

You could try as well one of my projects here: https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/TWR-52259

I hope this helps,

Erich

0 Kudos
Reply

2,945 Views
guilongxiao
Contributor I

I am sure that the cpu selected correct,and the board is ok.In order to make you a better analysis,I copy the console,as the following.

Starting 3rd party flash programming...

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

INF: Copyright 2012 P&E Microcomputer Systems,Inc.

INF: Command Line :"D:\Freescale\CW MCU v10.6\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0

INF: CMD>RE

INF: Initializing.

INF: Device Debug Module : Revision B+

INF: Device Detected : 5225x

INF: Target has been RESET and is active.

INF: CMD>CM D:\Freescale\CW MCU v10.6\MCU\bin\Plugins\support\coldfire\gdi\P&E\freescale_52259_1x32x128k.cfp

INF: Initializing.

INF: Device Debug Module : Revision A

INF: Device Detected : Generic 52xx

INF: Device Debug Module : Revision A

INF: Device Detected : Generic 52xx

INF: Not able to access processor. Try software reset. 

ERR: Error loading programming algorithm - load aborted.

0 Kudos
Reply

2,945 Views
BlackNight
NXP Employee
NXP Employee

I think your problem is that it does *not* properly detect the device. It says "INF: Device Detected : Generic 52xx" for you.

Below is what I have:

Starting 3rd party flash programming...

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_OK

INF: Copyright 2012 P&E Microcomputer Systems,Inc.

INF: Command Line :"C:\Freescale\CW MCU v10.6\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0

INF: CMD>RE

INF: Initializing.

INF: Device Debug Module : Revision B+

INF: Device Detected : 5225x

INF: Target has been RESET and is active.

INF: CMD>CM C:\Freescale\CW MCU v10.6\MCU\bin\Plugins\support\coldfire\gdi\P&E\freescale_52259_1x32x128k.cfp

INF: Initializing.

INF: Device Debug Module : Revision B+

INF: Device Detected : 5225x

INF: Initialized.

INF: ;version 1.01, 10/01/2008, Copyright P&E Microcomputer Systems, www.pemicro.com [522xx_512k]

INF: ;device Freescale, 52259, 1x32x128k

INF: ;begin_cs device=$00000000, length=$00080000, ram=$10000000

INF: Loading programming algorithm ...

INF: Done.

INF: CMD>EM

INF: Erasing.

INF: Module has been erased.

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DO_PARTITIONING, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

INF: CMD>PM

INF: Programming.

INF: Processing Object File Data ...

INF: .

INF: Programmed.

INF: CMD>VC

INF: Verifying object file CRC-16 to device ranges ...

INF:    block 00000000-000002FF ...

INF: Ok.

INF:    block 00000400-00000417 ...

INF: Ok.

INF:    block 00000420-00021ED7 ...

INF: Ok.

INF:    Checksum Verification Successful. (Cumulative CRC-16=$90BC)

INF: CMD>RE

INF: Initializing.

INF: Device Debug Module : Revision B+

INF: Device Detected : 5225x

INF: Target has been RESET and is active.

Below are screenshots of my settings. Can you verify them?

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

Erich

0 Kudos
Reply

2,945 Views
guilongxiao
Contributor I

1.png2.png3.png

0 Kudos
Reply

2,945 Views
guilongxiao
Contributor I

I check my settings as above.Do you have any advices?

0 Kudos
Reply

2,945 Views
BlackNight
NXP Employee
NXP Employee

Is your board the TWR-52259 or a custom board?

0 Kudos
Reply

2,945 Views
guilongxiao
Contributor I

Custom board.

0 Kudos
Reply

2,945 Views
BlackNight
NXP Employee
NXP Employee

Can you try it with the TWR-52259 board? Bottom line is that I think you have a board/hardware issue.

0 Kudos
Reply