Error while connecting to the interface hardware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error while connecting to the interface hardware

1,333 次查看
bisbe
Contributor I

Hello

 

I am trying to Run a project using a MultiLink Universal. I tried to Run the project in several boards, some own boards and some Demoboards (FRDM-K20D50M) and in all the cases the problem is the same. I attach a Screenshot of the error that appears. In the case of the Demoboards if I program the boards using the OpenSDA the boards works properly.

 

Any solution?

 

Best regards,

 

Sergi Bisbe

标签 (1)
0 项奖励
回复
1 回复

1,240 次查看
trytohelp
NXP Employee
NXP Employee

Hi Sergi,

Based on following configuration:

      - Windows 7 32 bit

      - CW for MCU V10.6

      - TWR-K70F120M

      - interfaces: P&E Multilink Universal, JLink and OSBDM.

With the Project wizard I've created an application based on TWR-K70F120M (PK70FN1M0) for the 3 interfaces.

After to have build the project, I'm able to load and debug the application with all interfaces.

However to be running the OSBDM must be plugged (it will provide the power supply required for the board).

Attached you will find the project used.

Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复