Error retreving content description for resource XXXXX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error retreving content description for resource XXXXX

1,499 次查看
528887301
Contributor II

When I import project MM9Z1J638-Demo-APPSW through cw11, I have this problem. What is the possible reason?

Error retreving content description for resource  XXXXX

MM9Z1J638-Demo-APPSW:KIT9Z1J638EVM | EVK MM9Z1J638, Battery Sensor with CAN/LIN | NXP 

2020-04-21_235825.png

0 项奖励
回复
1 回复

1,410 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

Please make sure the "Copy projects into workspace" check box is unchecked when importing the project.

 pastedImage_2.png

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复