Error retreving content description for resource XXXXX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error retreving content description for resource XXXXX

1,527件の閲覧回数
528887301
Contributor II

When I import project MM9Z1J638-Demo-APPSW through cw11, I have this problem. What is the possible reason?

Error retreving content description for resource  XXXXX

MM9Z1J638-Demo-APPSW:KIT9Z1J638EVM | EVK MM9Z1J638, Battery Sensor with CAN/LIN | NXP 

2020-04-21_235825.png

0 件の賞賛
返信
1 返信

1,438件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

Please make sure the "Copy projects into workspace" check box is unchecked when importing the project.

 pastedImage_2.png

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信