Error launching FRDM-K64F_MQXL_FLASH_OpenSDA ARM GDI Protocol Adapter : Can't connect. The Debugger can not connect to the P&E device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error launching FRDM-K64F_MQXL_FLASH_OpenSDA ARM GDI Protocol Adapter : Can't connect. The Debugger can not connect to the P&E device

2,072件の閲覧回数
michaelsmorto
Contributor IV

I am trying to compile and flash the NXP sensor funsion rev 5 and trying to following the instructions using a K64f freedom board with codewarrior 10.7 (latest one just downloaded for windows 7.  I am using the opensda and receiving the following error when I do a run configuration:

 

Error launching FRDM-k64F_MQLX_FLASH_OpenSDA ARM GDI Protocol Adapter.  Cannot connect . The Debugger can not connect to the P&E Device.

 

I have no idea what I am doing as this is my first experience with MBED - coming from a Arduino background.  So keep it simple

 

 

THanks

Mike

ラベル(1)
タグ(2)
3 返答(返信)

1,661件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I suggest you check the problem with below steps.

1. create a new work space.

2. create a new project in this workspace, test if the connection can work.

3. if it fails connection in step2, please update the FRDM board driver with referring this article

https://community.nxp.com/docs/DOC-105199 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,661件の閲覧回数
michaelsmorto
Contributor IV

Jennie

Your post helped alot.  It appears that if I use CodeWarrior I have to use segger   and if I want the board to act like a drive like for the sensor toolbox v5 I need to set it up like mned and just let it load the bin.  Broke the code with your help.

Thanks

Mike

0 件の賞賛
返信

1,661件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Mike,

Good to know. You are welcome!

Best Regards,

Jennie

0 件の賞賛
返信