;
; Add the ICR value to a constant offset and store in the OCR.
;
lda TPMC1V+1 ; 3 get the ICR value, low byte
add #LOW(time_base) ; 2 add low byte of update rate
tax ; 1 set aside for load
lda TPMC1V ; 3 get the ICR value, high byte
adc #HIGH(time_base) ; 2 add high byte of update rate
sta TPMC0V ; 3 high byte must always be loaded first
stx TPMC0V+1 ; 3 low byte must always be loaded last
; = 17 cycles
Hello FC,
A slight variation of Rocco's method that does not use the HIGH and LOW directives (not necessarily available for all assemblers).
lda TPMC1V+1 ; 3 get the ICR value, low byte
add #(time_base%256) ; 2 add low byte of update rate
tax ; 1 set aside for load
lda TPMC1V ; 3 get the ICR value, high byte
adc #(time_base/256) ; 2 add high byte of update rate
sta TPMC0V ; 3 high byte must always be loaded first
stx TPMC0V+1 ; 3 low byte must always be loaded last
Regards,
Mac
Thanks for the responses. I forgot to mention that its for the HCS08.
The assembler for CW 5.0 returns an error when the +1 is next to channel register. I have seen :smileyshocked: and :1 used before, what does the CW 5.0 assember use?
CompilerGuru wrote:
To access a low byte from a 16 bit variable from assembly, just add 1 to the address of the variable. The HC08 is big endian, and therefore the low byte is at the higher address.
Hmm . . . I could never get CW to work, so I'm still using MCUez. I wonder if this is why CW gives me thousands of errors? Sorry I can't be of more help there. Please let me know what you find out.
FC wrote:
The assembler for CW 5.0 returns an error when the +1 is next to channel register. I have seen :smileyshocked: and :1 used before, what does the CW 5.0 assember use?
;
; Add the ICR value to a constant offset and store in the OCR.
;
lda TPMC1V+1 ; 3 get the ICR value, low byte
add #LOW(time_base) ; 2 add low byte of update rate
sta TPMC0V+1 ; 3 load low byte of OCR
lda TPMC1V ; 3 get the ICR value, high byte
adc #HIGH(time_base) ; 2 add carry and high byte of update rate
sta TPMC0V ; 3 load high byte of OCR
; = 16 cycles
Hello Rocco, FC,
I have not been able to replicate FC's problem using CW 5.0 assembler. The arithmetic on the register address seems to work fine. I even added spaces before and after the + sign, again without problem (I thought I might have to add parenthesis in this case). In fact, when I placed a colon in lieu of the + sign, I got an assembly error.
I assume that FC is actually using the assembler, rather than inline assembly within the C compiler. The attached sample file assembles correctly using CW 5.0.
Regards,
Mac
;
; Add the ICR value to a SMALL constant offset and store in the OCR.
;
ldhx TPMC1V ; 4 Get the ICR value
aix #time_base ; 2 Add a small offset to it
sthx TPMC0V ; 4 And store in the OCR
; =10 cycles